Siemens Training Nederland
Den Haag
Prinses Beatrixlaan 800
2595 BN Den Haag
Zoetermeer
Werner von Siemensstaat 1
2712 PN Zoetermeer
Netherlands
Tel: +31 (0) 70 333 3900
Email: siemens.training.nl@siemens.com
This in principle 2-day long course is meant to learn methods to be able to analyse network faults when a SIPROTEC device has registered them.
The main purpose of the training is to teach all users of SIEMENS SIPROTEC protection devices to be able to read out and interpret the network faults that have occurred if a SIPROTEC protection system has detected a network fault using the recorded data in the digital relay.
Day 1: This is done in several steps, so that the first line recognition can be done by technical employees such as Mechanics or other employees working directly with the data from the LEDs and the data present in the display of the protection. But also, by being able to manually extract the relevant data from the last fault from the relay in a second step. Day 2: In addition, the additional data that may be present in the relay via a PC is discussed to be able to make a specialized analysis.
Type | Face-to-face training |
Duration | 2 days |
Language | nl |
All individuals involved in the operation of electrical installations who wish to gain more knowledge on how to recognize network faults within digital protections and how to read and analyze them. This includes engineers, commissioning personnel, and maintenance technicians.
Day 1:
Day 2:
Participants are expected to have basic knowledge of Energy Technology or at least an affinity for it. If attending the second day, participants must have completed the first Day of the course.
Face-to-0face