Siemens Training Nederland
Den Haag
Prinses Beatrixlaan 800
2595 BN Den Haag
Zoetermeer
Werner von Siemensstaat 1
2712 PN Zoetermeer
Netherlands
Tel: +31 (0) 70 333 3900
Email: siemens.training.nl@siemens.com
This course is intended for individuals who want to prepare automated tests for transformer differential protections and distance protections, which can then be performed by themselves or others. These individuals want to be able to convert protection settings into well-functioning and reliable test files.
If the participants are from the same company, other in-depth topics such as xRIO connections can also be covered. This can always be indicated in advance when requesting the course.
| Type | Face-to-face training |
| Duration | 2 days |
| Language | en, nl |
This course is meant for all persons that need to be able to perform tests on digital distance and transformer differential protection relays using a CMC testing unit from Omicron with the program TestUniverse. Engineers, commissioning engineers and maintenance technicians.
From the participant it is expected to have more advanced knowledge of digital protections and that the basic OMICRON training has been done.