My Dashboard

Training Support Office

Siemens Training Nederland

Contact

Den Haag
Prinses Beatrixlaan 800
2595 BN Den Haag
Zoetermeer
Werner von Siemensstaat 1
2712 PN Zoetermeer
Netherlands

Tel: +31 (0) 70 333 3900
Email:

SIPROTEC 4/5 Current transformare Earthing (H-SIP5CT)

  • In this optional course of about 2 hours you will learn how within the SIPROTEC range from the past to today the direction of the CT is determined by the indicated earthing of these CTs. Direction requires both voltage connections and current connections, within SIEMENS protections the motor convention is applied to determine this direction. As is common with most protection relay vendors.

Type Face-to-face training
Duration 1 day
Language en, nl

Target Group

  • This course is intended for persons involved in the engineering process, the determination of the settings, the programming, and the use of the protections of the entire SIPROTEC series. Engineers, commissioners and maintenance technicians.

Content

  • The Motor, Transformer or outgoing facing bay. Ct direction Line or the object to be protected.
  • CT towards the rail or opposite to the object to be protected.
  • CT, reason grounding.
  • Direction from Uen I to the SIPROTEC.
  • SIPROTEC 5 connections.
  • Standards combined in the drawings.
  • CT Towards the rail or away from the object to be monitored.
  • Enumeration of directions, directions, and display P.
  • Drawings of an installation Example 1.
  • Secondary tests:
    • +P star point towards the cable or the object to be protected.
    • -P star point towards the cable or the object to be protected.
    • +P star point towards rail or not towards the object to be protected.
    • -P star point towards rail or not towards the object to be protected.
  • Testing SIPROTEC 5 example.
    • Standard connection to the object: Yes.
    • Standard connection to object: No.
  • Generator and motor convention.
  • SIPROTEC solution.
  • SIPROTEC 5 special feature choice X or I.
  • Generator protection special.
  • Prerequisites

    • Basic knowledge of the different types of protection as covered in the H-BM or H-BI course. Knowledge of SIPROTEC 5 and DIGSI 5 as covered in the SIPROTEC 5 Basic Course with DIGSI 5.

    Note

      1. This optional course is intended to deepen the knowledge of how the directions around current transformers are determined within the complete SIEMENS SIPROTEC range. We have noticed that many users sometimes struggle with this. This course contains a lot of theory but can be deepened by giving real applications and examples with existing SIPROTEC models to support the theory. Then the course will take longer than the indicated 2 hours.
      2. If you also want to actively program yourself, we can add a separate practice part of the day where you can work with a security and your own data for this lockout function and a training PC or your own PC, provided that the correct software is installed on it. Together with an OMICRON for performing the tests.
      3. This course can be scheduled from 4 people. For more information or special requests, please contact the Power Academy.

    Downloads

    Contact