Siemens Training Nederland
Den Haag
Prinses Beatrixlaan 800
2595 BN Den Haag
Zoetermeer
Werner von Siemensstaat 1
2712 PN Zoetermeer
Netherlands
Tel: +31 (0) 70 333 3900
Email: siemens.training.nl@siemens.com
In this two-day course, you will learn how to work with the DIGSI 5 software package on your PC and how to handle various devices (protection devices) from the SIPROTEC 5 series. During this course, the selection and the way of programming a SIPROTEC 5 relay using DIGSI 5 will be explained. In addition, using a SIPROTEC 5 protection device present, it will be shown how the hardware is structured and how data can be read and analyzed in communication with this unit.
The course is not directly aimed at the functionality of a protection device or the choice of settings, although we will discuss some aspects of an example. There are product-specific courses for that. You will learn the features of the DIGSI 5 tool and become familiar with the characteristics of the SIPROTEC 5 hardware properties.
Type | Face-to-face training |
Duration | 2 days |
Language | en, nl |
This course is meant for persons involved with the engineering process, the determination of settings, programming, and using protections of the SIPROTEC 5 range. Engineers, commissioning engineers and maintenance technicians.
For the participants it is expected to be familiar with the base functions of digital protection equipment as also presented in the H-BIE training.
Face-to-face