My Dashboard


My Profile

Training Support Office

Siemens Training Nederland

Contact

Den Haag
Prinses Beatrixlaan 800
2595 BN Den Haag
Zoetermeer
Werner von Siemensstaat 1
2712 PN Zoetermeer
Netherlands

Tel: +31 (0) 70 333 3900
Email:

ANSI 87 Line Differential Protection in SIPROTEC 5. (H-SIP5LB)

  • In this 1-day course, you will learn how to use DIGSI 5 to implement line differential protection as a protection function for monitoring lines and cables using two communication-linked SIPROTEC 5 line differential protections for the SIPROTEC 5 protections. This course focuses on the protection function itself, the settings that can be made and their meanings. It also covers how to practically test this function with an OMICRON test kit and how to handle the online display of the measurements.

Type Face-to-face training
Duration 1 day
Language nl

Target Group

  • This course is intended for individuals involved in the engineering process, determining settings, programming, and reading line differential protections of the SIPROTEC 5 series. Engineers, commissioning personnel, and maintenance technicians.

Content

  • Theory of Line Differential Protection:

    • The general principle.
    • Stabilization, restraint, or bias of transformer differential.
    • Line differential protection.
    • Structure of the function and logical setup.
    • ANSI87L communication is part of the line differential.
    • SIPROTEC 5 stabilization of line differential.
    • Idiff> Vector comparison with renewed Fourier filters.
    • Current transformer fault stabilization.
    • Idiff> CT (saturation) detector stabilization.
    • Measurement value transfer synchronization.
    • Setting steps DIGSI 5 and DIGSI 4.
    • A transformer within the protected object.
    • Load current stabilization I-diff limit.
    • Inrush stabilization 2nd HH method. Transformer in the diff area or directly nearby.
    • Response to higher harmonics.
    • Inrush phenomena.
    • Overexcitation and saturation.
    • CWA inrush recognition. Transformer in the diff section or directly nearby.
    • Idiff and I-diff fast or I-diff fast 2 (>=CP300).
    • Monitoring the differential current.
    • Intertripping
  • Introduction to settings for a cable or line.
  • General settings of the line differential.
  • Idiff setting of the line differential.
  • Idiff fast 2 setting of the line differential.
  • Idiff fast setting of the line differential.
  • Carryover setting of the line differential.
  • Pickup and operate of the line differential.
  • Disabling or logging out of the local line differential.
  • Stationary differential current.
  • Idiff fast or I-diff fast 2 setting (Qdiff).
  • Example settings with transformer.
  • Multi-legged differential.
  • Setting data in SIPROTEC 5.
    • Hardware.
    • LEDs.
    • CT/VT connections.
    • Function group connections.
    • Power system data.
    • Line protection general.
    • Inrush detection or Closure Detected Line Protection.
    • Line protection.
    • Idiff Fast2.
    • Intertripping
  • Setting data for necessary communication.
    • Time synchronization of differential communication.
    • Variants of differential communication.
    • Structure of classical differential communication.
    • Direct communication.
    • Communication via multiplexing.
    • Communication via media.
    • Differential communication SIPROTEC 4 and 5.
    • Structure of extended differential communication.
    • Extended communication via UART.
    • Extended communication via Ethernet-BD.
    • Protection communication Type 1.
    • External synchronization.
    • Linking protection to communication.
    • Internal "External" synchronization.
    • Setting data IP example.
    • Hardware setting PPS synchronization USART setup.
    • Prot.com. (Type 1) example.
    • Display example.
  • Testing.
  • Examples, applications, tips.
    • Line differential protection in combination with a SIPROTEC 5 and a SIPROTEC 4 protection.

    Prerequisites

    • Basic knowledge of the different types of protections as covered in the H-BM or H-BI course. Knowledge of SIPROTEC 5 and DIGSI 5 as covered in the SIPROTEC 5 Basic Course with DIGSI 5.

    Note

      • This course is based on the specific line differential protection within SIPROTEC 5 and contains a lot of theory. Therefore, it is more about following along rather than actively participating on your own or a training PC.
      • If you also want to actively program, we can add a separate practical day where you can work with a line differential protection and a training PC or your own PC, provided the correct software is installed.
      • For testing the line differential protection, a separate day for an additional session of the OMICRON course is recommended.
      • This course can be scheduled for groups of 4 or more people. For more information or special requests, please contact the Power Academy.

      Downloads

      Contact