Информация для Заказчика:
Teл.: +7 (495) 737-1-737
E-Mail:

|
  1. Курсы
  2. SINUMERIK
  3. NC-SMILLBP - Описание

Курс NC-SMILLBP / NC-SMILLBP (NC-SMILLBP)

  • This course is designed for operators/skilled workers who are experienced in the operation of a CNC milling machine. DIN-ISO knowhow is not required for this course. On completion of the course, the participant will be able to create a program using graphical programming with ShopMill. The content of this course will be transmitted theoretically by means of the Sinutrain training software that is identical to that of the controller, as well as practically using a machine tool.

    Для бронирования данного курса просим перейти по ссылке и заполнить анкету: https://di-events.siemens.ru/courses/
Тип Очный тренинг
Продолжительность 4 Дн.
Язык ru

Целевая группа

  • Programmers
  • Commissioning engineers
  • Operators

Содержание

  • - Introduction to the functionality and the controller
  • - Introduction to tool management
  • - Introduction to the manual operating area
  • - Introduction to creating, testing, modifying and saving programs
  • - Programming with standard milling cycles
  • - Programming free contours using the contour calculator
  • - Centering, drilling, thread cutting
  • - Working with the function "Multiple clamping"
  • - Programming with subroutines
  • - Working with transformations

Требования к участнику

  • Basic knowledge of automatization

Downloads