Settings for Microsoft Internet Explorer
Javascript
To change the JavaScript settings in the Internet Explorer, please activate the “Tools“ – “Internet Options...“ menu. Then, please select the “Security“ tab. Choose the Internet icon and click on “Custom Level…“.
Under “Scripting“ / “Active Scripting“, click on “Enable“ and confirm your entry with ”OK“.
ActiveX
To change the ActiveX settings in the IE, please activate the ”Tools“ – ”Internet Options…“ menu. Then, please select the “Security“ tab. Choose theInternet icon and click on “Custom Level…“.
The settings should then appear as follows to enable the installation of the ActiveX components:
The settings should then appear as follows to enable the installation of the ActiveX components:
The “Download unsigned ActiveX controls“ can remain disabled.Then, restart the Browser.
Ask your System Administrator to make the setting changes for you if you don’t have the proper authorization.
Popup-Blocker
Clicking on the "go" button in the learning environment, activates an intermediate page. The Web Based Training module is opened in a new browser window. Should the window not open, please, first of all check whether one or more pop-up blockers are installed and activated on your computer. A pop-up blocker is normally included in the Windows XP Service Pack 2, for example. Various browser toolbars also contain a pop-up blocker. Please deactivate all pop-up blockers while you’re working with the module.
Example: Pop-up blocker in the Internet Explorer in Windows XP.
Click on the yellow bar and then on “Temporarily Allow Pop-ups“ or “Always Allow Pop-ups from This Site...“.
Update the site and once again click on the “go“ button.