+86 400 810 4288 转4号键

+86 400 810 4288 转4号键
Automated systems are becoming more complex and pervasive, and an increased knowledge is required to design, operate and maintain them than ever before. Complex mechatronic systems are the nexus of mechanical, electrical, and computerized technologies. There is a growing need for qualified people at all levels of an organization with knowledge of integrated mechatronic systems. Siemens, a world leader in mechatronic engineering, has responded to this need by creating an industry certification program to help students, teachers and institutions.
The Siemens Mechatronic Systems Certification Program (SMSCP) is a comprehensive industry skills certification in mechatronic systems. Offered together with partner schools worldwide the SMSCP is designed to be integrated into existing programs of study, and is divided into three exam-based levels. Each level is directly tied to a job profile that clearly defines the on-the-job competencies of certified personnel. A Siemens certification is world-class technical training.
Systems Approach
A central theme in the SMSCP is the Systems Approach, a special set of teaching and learning methods developed over 30 years ago in Siemens´ technical schools in Germany.
Under the Systems Approach, students learn about the complexities of a system in a holistic fashion.
Starting at the macro level, students first see the full system and learn about its function.
From there they go into one of the system modules, examining the components contained within the module and their inter-relationships with one another.
At the component or device level, students learn about the physical properties of each component in the system, and, coupled with their knowledge of the flow of energy and information within the system, they will learn to carry the measurements required to pinpoint where malfunctions are occurring. They can determine whether a component is defective, whether the energy or information flow is incorrect, or if the hardware of the control system is defective – in other words moving from the micro-level back up to the macro-level in the troubleshooting process.
As a result, Siemens Certified Mechatronic Systems Assistants, Associates and Professionals are equipped with troubleshooting strategies and are able to transfer their knowledge easily to other systems, resulting in flexible and autonomous employees.
Increase efficiency and productivity among machine operators, technicians and engineers
With its emphasis on in-demand industrial skills, troubleshooting, and hands-on practice, SMSCP’s training will provide you with knowledgeable workers, who are able to easily move into different job areas.
Companies and industries receive highly skilled technical workers while drawing on local education and training resources via partner schools. Our program partners offer the SMSCP training at a fraction of the cost of private training companies and in some areas, the training may qualify for funding from local government.
SMSCP的一个中心主题是系统学习法,这是30多年前在德国西门子技术学校开发的一套特殊的教学方法。在系统方法下,学生以整体方式了解系统的复杂性。从宏观层面开始,学生首先看到完整的系统并了解其功能。从那里,他们进入一个系统模块,检查模块中包含的组件以及它们之间的相互关系。在组件或设备级别,学生将了解系统中每个组件的物理属性,并结合他们对系统内能量和信息流的了解,他们将学习如何进行所需的检测,来对故障进行准确定位。他们可以确定组件是否有缺陷,能源或信息流是否正确,或者控制系统的硬件是否有缺陷。换句话说,在故障排除过程中从微观级别转移到宏级别。
因此,西门子认证的机电一体化系统助理,系统技师和工程师配备了故障排除策略,并能够轻松地将他们的知识转移到其他系统,成为技能知识灵活应用的员工。
认证能力范围
等级一 西门子认证机电一体化系统助理
教师认证2周(德国)
等级二 西门子认证机电一体化系统技师
教师认证2周(德国)
等级三 西门子认证机电一体化系统工程师
教师认证2周(德国、美国或加拿大)
认证合作价格(含6%增值税):
等级一和等级二教师认证:RMB 47,500元/周/人
等级三教师认证需单独报价
合作授权:RMB 50,670元/年